Lithium-ion Battery Technology Addresses the Two Biggest UPS Concerns: Battery Life and Weight Facebook LinkedIn Twitter Email Pankaj SharmaMay 23, 2018August 6, 2021 LinkedIn 9347 views TAGSend userpower protectionCertaintyLithium IonAPC Smart-UPSVRLA batterybattery lifebattery weight Historically, the most frequent issues customers have with uninterruptible power supplies (UPSs) have to do with two criteria: battery life and weight. But lithium-ion battery technology promises to bring welcome relief, because they last more than twice as long as traditional UPS batteries and weigh only about a third as much. Traditional UPS battery life UPSs typically use valve regulated lead acid (VRLA) batteries which, under normal circumstances, last around 3 to 5 years. We say “around” because several variables can come into play to diminish battery life. One is the number of charge and discharge cycles to which the battery is subject. Each time the UPS kicks to life to back-up a load, it must discharge the battery. When its job is done, the UPS recharges the battery again. Each of these cycles takes a toll on the battery; any VRLA battery has only so many such cycles in its lifespan. Temperature can also be the enemy of VRLA batteries. High ambient temperatures will not only diminish the life of the battery but impact the battery performance overall. Either of these issues can serve to limit the life of a VRLA battery, forcing its replacement. And that can be an expensive proposition, requiring customers to not only pay for the new battery but also for the labor involved in replacing it. That’s especially true in a highly distributed environment, such as a company with numerous branch offices or retail locations. Why weight is an issue with UPSs VRLA batteries are also quite heavy. For a large UPS installation, that has implications including installation. It can take two or three people to install larger UPSs because the batteries weigh so much. Alternatively, you may be forced to remove the battery during installation. In either case, the labor costs are high. In some cases, customers may need to reinforce the flooring on which racks with many UPSs sit to support their weight. Here again, that becomes a costly endeavor. Lithium-ion: A better UPS battery option Lithium-ion batteries address both the lifespan and weight issues. First, Lithium-ion batteries last about twice as long as VRLA batteries, up to about 10 years. That is roughly the same as the expected lifespan of a UPS, which effectively means you never have to replace a Lithium-ion UPS battery. That’s true even at extreme temperatures because Lithium-ion batteries can operate at temperatures up to 40° C/104° F with no performance degradation. Secondly, Lithium-ion batteries weigh about 30% less than VRLA batteries. That can obviate the need for reinforced floors and makes installation far easier. All these benefits do come at a higher cost than VRLA batteries, but when you consider all the costs associated with VRLA batteries in terms of lifespan, maintenance and weight, APC Smart-UPS™ Lithium-ion based UPSs, as an example, offer about a 50% lower total cost of ownership (TCO). To learn more about the benefits of Lithium-ion batteries and how they can bring you Certainty in a Connect World, download the free white paper, “Battery Technology for Single Phase UPS Systems: VRLA vs. Li-ion.” We think you’ll agree that for many medium to large enterprise installations, Lithium-ion makes good business sense. Want to learn more? Assess the benefits of APC Smart-UPS with Lithium-Ion battery technology for your business.
I have a apc backup es500 but have lost the operating instructions. When I plug in the unit for prower protection it makes a buzzing noise. How do I know the unit I fully charged and protecting my device . Reply
Hi Steve, Thank you for reaching out. While there is some sound present with all UPS units, none of them should be obtrusively loud. It would be very helpful to know the exact model and serial of the UPS. This information can be found on a small white sticker with a bar code on the bottom of the unit. This would allow us to get you a link to the user’s manual. When you first turn on a Back-UPS unit, it will run a self test. If the UPS has a bad battery or some other issue, it will usually make a chirping or solid beep tone during the self test. If it completes the self test without issue, it should be able to provide battery back up and surge protection as expected. If you still have concerns, it might be good to contact local CCC in your country. You can find contact information for all regions here: https://www.apc.com/support/contact-us/index.jsp Reply
Believe it or not, a revolution in lithium ion batteries is in its final stages now. The use of polymer electrolytes was a dramatic innovation in lithium ion batteries that has enabled the proliferation of smartphones, tablets, and ultrabooks. A quick trip through one history of polymer electrolytes (there is a parallel but hard to research second history within the major Japanese conglomerates) will illustrate the timescales for battery commercialization. Reply