Smart Surge Protectors Offer Smart Home Features – at a Fraction of the Cost Facebook LinkedIn Twitter Email Pankaj SharmaApril 26, 2019 LinkedIn Viewed: 3781 TAGSsmart homepower surgeAlexasmart surge protector Probably you’ve seen ads or web sites for all kinds of smart home and office features, such as light bulbs you can turn on and off from afar, voice-controlled TVs and the like. It all sounds great, like the Jetsons come to life – and then you see the price tag. Well, there’s another way to get similar functionality without replacing all your existing lights, entertainment gear and appliances: smart surge protectors. Surge protectors are a must-have for any home or home office, as they protect sensitive equipment from short bursts of power that are higher in voltage than the devices can handle. Surges can result from a number of causes, including outside utility work, lightning strikes and other weather events, even the normal operation of appliances like refrigerators and air conditioners as they cycle on and off. Today some smart surge protectors are adding even more value because they have the ability to connect to Wi-Fi networks in your home and/or home office and be controlled by a smart phone app or Alexa. On these emerging surge protectors, some ports will be “smart” ports, able to be remotely controlled. Plug a lamp into these ports, and you’ll be able to turn it off and on from wherever you may be. Let’s say you and your spouse are out for dinner with friends on a Saturday night. Your teenage kids are home, under strict orders to shut off the TV and head to bed at 10 p.m. When the appointed hour comes, you can check your phone and see whether the TV outlet is live. If so, you can remotely turn it off. You could also use it to program the smart surge protector to shut off the TV outlet at a certain time even when you’re watching. Smart Surge Protector = Cost Savings Cost savings is also a significant benefit of a smart surge protector. Consider the devices in your home office, including your computer, monitor and printer. As long as they’re plugged in, they all draw small amounts of “vampire” power even when they’re not on. Plug them into a smart outlet and you can program it to shut down power completely, such as at night and on weekends. (Just make sure you turn your computer off first to avoid a hard shutdown.) The same goes for your TV and entertainment systems– if they’re not being used, you can ensure they don’t draw any power. Many homes routinely run dehumidifiers in summer months, to prevent mold, mildew and foul odors. Typically, they’re in the basement – out of sight, out of mind – probably running 24×7. Plug it into a smart outlet and you can schedule them to run maybe 6 hours or so during the day and see if that’s enough to do the job. If so, you’ll save a lot of power. Or consider UV lights that gardeners use to grow plants from seed indoors. A smart surge protector would allow the lights to be scheduled to turn on and off at appropriate times, and to turn them on remotely as needed. Home Security and Convenience Smart outlets can also be used to provide a level of security to your home, with apps that can schedule when different surge protector outlets turn on or off. Plug a lamp or two into a smart outlet and when you’re away you can program the lamps to turn on at dusk and off at your normal bedtime – from wherever you may be. It’s a whole lot easier than fumbling with those rotary timers, and nowhere near as expensive as buying individual “smart” lightbulbs. There’s a convenience factor, too. Plug your coffee maker into a smart outlet and you can schedule it to start brewing in the morning, so you can wake up to fresh, hot coffee. A Smarter Surge Protector Not every surge protector has such features, of course, but one that does is the APC™ by Schneider Electric Smart Plug Surge Protector Power Strip. The device features six surge protected outlets, three of which are smart outlets, and four USB charging ports, two of them smart ports. That’s five smart, Wi-Fi-enabled ports on each strip. The smart outlets and ports can be controlled by Alexa voice commands or the APC Home App, available in both the Apple App Store and Google Play. The app enables you to turn them on and off at will, or to put them on a schedule. You can also group outlets and ports on different surge protectors to follow the same schedule – one light in the living room and another in a bedroom, for example. Not everyone is ready to shell out what it takes to create a truly “smart” home, and not everyone necessarily wants all those bells and whistles. But for a small investment, you can get many of the same features, while keeping your existing fixtures and appliances. Check out the Smart Plug Surge Protector Power Strip, available at Amazon, and I’ll bet you can think of many uses for it in your home or home office. Also, learn even more about how to ensure power protection and connectivity by exploring APC’s home solutions.
This surge protector has been challenging to connect to WiFi. I still can’t get it connected, so it isn’t “simple” to set up. Reply
We are sorry to see that you are experiencing issues connecting your new SmartSurge device to your WiFi network. It is difficult to say at which point during the install you are encountering the issue. There are several things which may cause difficulty during setup, for one example the SmartSurge is only enabled for 2.4GHz WiFi connections. It is also possible, however that the Network SSID was not initially verified during setup. You may attempt to add the device again by using the following steps; To reset the device, hold down the Outlet 1 button for 5 seconds. The Wi-Fi LED will flash amber. Navigate to the Device screen in the APCHome.app and re-add this device using the “+”. Follow the instructions to re-add the device using the new network SSID. All previous configurations will not be changed. At any point, please feel free to contact our Technical Support representatives for step-by-step assistance in your setup or if you have any additional issues or questions. Reply
Hi, does your product allow the power cycling of the router and cable modem? I am trying to manage a property remotely and sometimes I need to power cycle the modem / router combo. Obviously if I just turn them off, I lose the connection. Thanks Reply
The device will allow the user to enable or disable power to the outlets. As you’ve pointed out, turning off the Router and/or Modem will render the user unable to turn them back on remotely. There is currently no option in the APC Home app to cycle power to the receptacle, allowing the receptacle to turn itself and the connected equipment back on automatically. With that said, one feature of the APC Home app is the ability to schedule outlets On and Off. This would likely be the best option for managing your Router/Modem remotely. Reply