Why the Media and Entertainment Industry is Now Powered by Edge Computing

For the most part, the Internet of Things (IoT) works on the principle of gathering data from the many connected devices we all use on a daily basis.

New sources of data from connected IoT devices helps media companies enrich what they know about their audiences and influences how they present content directly to you. These data sources serve two roles, ensuring that the best performance is delivered in the moment, while over time serving as a data set providing analysis that will allow for even better performance and capabilities delivered because of these insights. This deeper insight helps them to develop better ways of influencing your behaviour as you consume content, across a much wider ecosystem of touchpoints. This ability, however, intensifies the media and entertainment industry’s dependency on data and on the systems, that gather, transport, process and store that data. Couple this trend with today’s societal demands on instantaneous connection and our zero tolerance for latency, and you find a media industry that, according to Accenture, is spending 54 percent more on IoT in the last three years.

To gain a better understanding of how IoT is impacting the industry, let’s take a look at the three most important pillars: content creation, distribution and consumption.

Content creation requires technological scalability

The level of complexity to produce advanced cinema has moved beyond the challenge of developing a well-executed art project. Engineering now plays a critical role, requiring increased levels of compute power to support media industry’s digital requirements. Consider, for example, Animal Logic, which is one of the world’s leading independent creative digital studios. Their production staff created over 600 visual effects in support of the 2013 film, “The Great Gatsby.”

Pulling off these visual effects requires a sophisticated technology backbone. Scalability of compute power physical infrastructure (servers, storage and the power and cooling that supports these IT systems) is one of the major challenges that growing studios face. Power and hardware needs to be engineered efficiently so that costs can be controlled and so that systems uptime can be maintained.

5G now impacts content distribution speed expectations

According to Ericsson, communications network operators will spend $1.7 trillion on equipment upgrades to support 5G between now and 2020. Everyone is expecting 5G network responsiveness to be high, and significantly exceed the speed and bandwidth of today’s 4G networks. If the physical infrastructure is not aligned to support the change, the network will fail. 5G communication is projected to perform upwards of 1000x faster than 4G. This means you’ll be able to download a full HD movie in a matter of seconds, versus the hour it may take on the 4G network of today.

But again, all of this won’t happen automatically. The ability to quickly download large quantities of data requires a physical infrastructure that can support edge computing, which implies small pockets of computer power and cooling infrastructure located physically close to end users. Fortunately, cell towers have the existing space that is already safe, secure and wired to support the small data centres that are required. Edge computing will enable local storage of copies of the entire content library, for example.

Content consumers will not tolerate latency

According to Google, 53 percent of mobile users abandon sites that take over 3 seconds to load. None of us can stand waiting for our iPad screens to respond to our touch. Content consumption habits, for business-critical transactions and entertainment alike, require instantaneous data transfer. If we experience too many loading delays…game over. However, these latency issues cannot be resolved by far off cloud data centres. Edge computing facilities will need to be deployed for content speeds to meet consumer expectations.

Adjustments on the technological back end will need to be made for users to get the device response speeds they demand for both business critical and entertainment data consumption. Both edge data centres, the size of a small bedroom, and large cloud data centres will need to work together in a hybrid ecosystem.

In all three of these key media industry business processes, the technology “back-end” plays a critical role. Companies like Schneider Electric both provide expertise in designing, building, operating and maintaining high availability edge computing infrastructure.

For more information on APC by Schneider Electric infrastructure solutions contact us on 1800 652 725 or visit www.apc.com/au/

 

Leave a Reply

Your email address will not be published.