Hyper-converged IT Infrastructure: A Sound Solution for Keeping up with Data Growth in the IoT Era

Hyper-converged Infrastructure (HCI) isn’t new. It’s existed for some time. It saw early popularity in virtual desktop applications. But it’s now being used by many companies to support data centre consolidation efforts.

The quest for increased simplicity, efficiency, and agility, coupled with hybrid deployments and IT virtualisation refresh cycles, is driving enterprises to hyper-converged IT. At Schneider Electric, we are also seeing increased interest and adoption at the edge due to IoT and data processing needs.

HCI blends traditional three-tier architecture (compute, storage, and networking) into a single software-defined solution. It greatly simplifies configuration and achieves high performance.

Rationale for hyper-converged infrastructure: continued explosion in IoT leading to massive data generation

As the Internet of Things (IoT) phenomenon continues unabated, contributing to a massive influx of data that companies must process, these same companies will increasingly rely on hyper-converged infrastructure.

The increase in data generation is expected to continue and grow dramatically. The research firm IDC “predicts that by 2025 there will be 55.7B connected devices worldwide, 75% of which will be connected to an IoT platform. IDC estimates data generated from connected IoT devices to be 73.1 ZB by 2025, growing from 18.3 ZB in 2019. Most of this data arises from security and video surveillance, but Industrial IoT applications will also take a significant portion of this data.”

Enabling hyper-converged infrastructure at the edge

“By 2025, over 30% of HCI units will be deployed at edge locations, which is a substantial increase from fewer than 15% in 2020.”

To keep pace with this migration to the edge, data centres will need to become more agile and cost-effective. This is precisely where hyper-converged IT infrastructure can leverage integrated physical infrastructure in the form of micro data centres.

Hyper-converged infrastructure is an extension of converged infrastructure, where all servers, storage, and networking components are delivered in a single enclosure – complete with hypervisor and management software.

Schneider Electric’s EcoStruxure Micro Data Centres are a good example of solutions which have been designed in collaboration with leading hyper-converged IT partners. They include enclosures, back-up power (uninterruptible power supply), cooling, security, environmental monitoring, and remote management with diagnostics.

These micro data centre designs come in reference designs, including hyper-converged IT from leading IT vendors – HPE SimpliVity, Scale, StorMagic, Nutanix, Dell VxRail, and Cisco Hyperflex. They can also be configured through our digital configuration tool, assembled, and delivered through one of our integration partners.

This makes it fast, simple, and cost effective to design, procure and deploy a complete hyper-converged micro data centre solution.

Hyper-converged infrastructure ensures business continuity

Another key benefit of such self-contained systems: they’re easy to transport. That can be critical in the wake of a natural disaster, after a merger or acquisition, or just when it’s time to move to a new site.

There’s no question the IoT era brings with it some exciting opportunities for businesses to extract value from data like never before – if they have the appropriate IT infrastructure.

It’s equally clear that hyper-converged IT infrastructure, combined with EcoStruxure Data Centre solutions, deliver a sound answer for organisations of almost any size, providing the sort of agility and effectiveness the IoT era demands.

To learn more about Schneider Electric’s converged and hyper-converged IT infrastructure solutions for data centres, please click here.

Leave a Reply

Your email address will not be published. Required fields are marked *