Lithium-ion Battery Technology Addresses the Two Biggest UPS Concerns: Battery Life and Weight

Historically, the most frequent issues customers have with uninterruptible power supplies (UPSs) have to do with two criteria: battery life and weight. But lithium-ion battery technology promises to bring welcome relief because they last more than twice as long as traditional UPS batteries and weigh only about a third as much.

meeting

Traditional UPS battery life 

UPSs typically use valve regulated lead acid (VRLA) batteries which, under normal circumstances, last around 3 to 5 years. We say “around” because several variables can come into play to diminish battery life.

One is the number of charge and discharge cycles to which the battery is subject. Each time the UPS kicks to life to back-up a load, it must discharge the battery. When its job is done, the UPS recharges the battery again. Each of these cycles takes a toll on the battery; any VRLA battery has only so many such cycles in its lifespan.

Temperature can also be the enemy of VRLA batteries. High ambient temperatures will not only diminish the life of the battery but impact the battery performance overall.

Either of these issues can serve to limit the life of a VRLA battery, forcing its replacement. And that can be an expensive proposition, requiring customers to not only pay for the new battery but also for the labor involved in replacing it. That’s especially true in a highly distributed environment, such as a company with numerous branch offices or retail locations.

Why weight is an issue with UPSs 

VRLA batteries are also quite heavy. For a large UPS installation, that has implications including installation. It can take two or three people to install larger UPSs because the batteries weigh so much. Alternatively, you may be forced to remove the battery during installation. In either case, the labor costs are high.

In some cases, customers may need to reinforce the flooring on which racks with many UPSs sit to support their weight. Here again, that becomes a costly endeavor.

Lithium-ion: A better UPS battery option 

Lithium-ion batteries address both the lifespan and weight issues.

First, Lithium-ion batteries last about twice as long as VRLA batteries, up to about 10 years. That is roughly the same as the expected lifespan of a UPS, which effectively means you never have to replace a Lithium-ion UPS battery. That’s true even at extreme temperatures because Lithium-ion batteries can operate at temperatures up to 40° C/104° F with no performance degradation.

Secondly, Lithium-ion batteries weigh about 30% less than VRLA batteries. That can obviate the need for reinforced floors and makes installation far easier.

All these benefits do come at a higher cost than VRLA batteries, but when you consider all the costs associated with VRLA batteries in terms of lifespan, maintenance, and weight, APC Smart-UPS™ Lithium-ion based UPSs, as an example, offer about a 50% lower total cost of ownership (TCO).

To learn more about the benefits of Lithium-ion batteries and how they can bring you Certainty in a Connect World, download the free white paper, “Battery Technology for Single Phase UPS Systems: VRLA vs. Li-ion.” We think you’ll agree that for many medium to large enterprise installations, Lithium-ion makes good business sense. Want to learn more? Assess the benefits of APC Smart-UPS with Lithium-Ion battery technology for your business.

Leave a Reply

Your email address will not be published. Required fields are marked *

This site uses Akismet to reduce spam. Learn how your comment data is processed.